ZPS_tsAfNwkLeaveIndEvent
This structure is used in the ZPS_EVENT_LEAVE_INDICATION event, which indicates that a neighboring node has left the network or a remote node has requested the local node to leave.
The ZPS_tsAfNwkLeaveIndEvent
structure is detailed below.
typedef struct {
uint64 u64ExtAddr;
uint8 u8Rejoin;
} ZPS_tsAfNwkLeaveIndEvent;
where:
u64ExtAddr
is the 64-bit IEEE (MAC) address of the node that has left the network, or is zero if the local node has been requested to leave the networku8Rejoin
indicates whether the leaving node was requested to attempt a subsequent rejoin of the network:zero represents FALSE
a non-zero value represents TRUE.
Parent topic:Event structures