ZPS_tsAfPollConfEvent
This structure is used in the ZPS_EVENT_NWK_POLL_CONFIRM event, which reports the completion of a poll request sent from the (local) End Device to its parent.
The ZPS_tsAfPollConfEvent
structure is detailed below.
typedef struct {
uint8 u8Status;
} ZPS_tsAfPollConfEvent;
where u8Status
is one of the status codes from the lower stack layers, detailed in Section 11.2.
Parent topic:Event structures