ZPS_tsAplApsKeyDescriptorEntry

This structure contains a link key for secured communications with another node.

typedef struct
{
    uint32     u32OutgoingFrameCounter;
    uint16     u16ExtAddrLkup;
    uint8      au8LinkKey[ZPS_SEC_KEY_LENGTH];
} ZPS_tsAplApsKeyDescriptorEntry;

where:

  • u32OutgoingFrameCounteris the outgoing frame counter value which is incremented on each transmission to a destination address below.

  • u16ExtAddrLkupis the index of the local look-up table entry that contains the IEEE/MAC address of either the Trust Centre or the target node.

  • au8LinkKey[]is an array containing the link key.

Parent topic:Other structures