ZPS_tsAplZdpDeviceAnnceReq

This structure is used by the function ZPS_eAplZdpDeviceAnnceRequest(). It represents an announcement that the sending node has joined or rejoined the network.

The ZPS_tsAplZdpDeviceAnnceReqstructure is detailed below.

typedef struct { uint16 u16NwkAddr; uint64 u64IeeeAddr;

uint8 u8Capability;

} ZPS_tsAplZdpDeviceAnnceReq;

where:

  • u16NwkAddris the network address of the sending node

  • u64IeeeAddris the IEEE address of the sending node

  • u8Capabilityis a bitmap representing the capabilities of the sending node. This bitmap is detailed in Table 1 in section ZPS_tsAfNwkJoinIndEvent.

Parent topic:ZDP Request structures