ZPS_tsAplZdpDiscoveryCacheRsp
This structure is used to store Discovery_Cache_rsp message data - a response to a call to the function ZPS_eAplZdpDiscoveryCacheRequest(). This response indicates that the sending node has a primary discovery cache.
The ZPS_tsAplZdpDiscoveryCacheRsp
structure is detailed below.
typedef struct {
uint8 u8Status;
} ZPS_tsAplZdpDiscoveryCacheRsp;
where u8Status
is the return status for ZPS_eAplZdpDiscoveryCacheRequest().
Parent topic:ZDP response structures