ZPS_tsAplZdpDiscoveryStoreRsp
This structure is used to store Discovery_Store_rsp message data - a response to a call to the function ZPS_eAplZdpDiscoveryStoreRequest(). This response indicates whether the sending node has successfully reserved space in its primary discovery cache.
The ZPS_tsAplZdpDiscoveryStoreRsp
structure is detailed below.
typedef struct {
uint8 u8Status;
} ZPS_tsAplZdpDiscoveryStoreRsp;
where u8Status
is the return status for ZPS_eAplZdpDiscoveryStoreRequest().
Parent topic:ZDP response structures