ZPS_tsAplZdpMgmtPermitJoiningRsp

This structure is used to store Mgmt_Permit_Joining_rsp message data - a response to a call to the function ZPS_eAplZdpMgmtPermitJoiningRequest(). This response is issued by a remote node (Router or Coordinator) that has been requested to enable or disable joining for a specified amount of time. The response is only sent if the original request was unicast (and not if it was broadcast).

The ZPS_tsAplZdpMgmtPermitJoiningRspstructure is detailed below.

typedef struct {
     uint8 u8Status;
} ZPS_tsAplZdpMgmtPermitJoiningRsp;

where u8Statusis the return status for the function ZPS_eAplZdpMgmtPermitJoiningRequest().

Parent topic:ZDP response structures