ZPS_tsAplZdpNwkAddrRsp
This structure is used to store NWK_addr_rsp message data - a response to a call to the function ZPS_eAplZdpNwkAddrRequest(). This response contains the network address of the node with a given IEEE address.
The ZPS_tsAplZdpNwkAddrRsp
structure is detailed below.
typedef struct { uint8 u8Status;
uint64 u64IeeeAddrRemoteDev;
uint16 u16NwkAddrRemoteDev;
uint8 u8NumAssocDev;
uint8 u8StartIndex;
/* Rest of the message is variable Length */
uint16* pNwkAddrAssocDevList;
} ZPS_tsAplZdpNwkAddrRsp;
where:
u8Status
is the return status for ZPS_eAplZdpNwkAddrRequest()u64IeeeAddrRemoteDev
is the IEEE address of the remote node that sent the response (this is the IEEE address specified in the original request)u16NwkAddrRemoteDev
is the network address of the remote node that sent the response (this is the network address that was requested)u8NumAssocDev
is the number of neighboring nodes for which network addresses are also being reported (in the remainder of the structure)u8StartIndex
is the index in the remote node’s Neighbor table of the first entry to be included in this report. This element should be ignored if the elementu8NumAssocDev
is 0.pNwkAddrAssocDevList
is a pointer to a list of 16-bit network addresses of the remote node’s neighbors (this is a variable-length list with four bytes per node). This element should be ignored if the elementu8NumAssocDev
is 0.
Parent topic:ZDP response structures