ZPS_tsAplZdpRemoveNodeCacheReq

This structure is used by the function ZPS_eAplZdpActiveEpStoreRequest(). It represents a request to a remote node to remove from its Primary Discovery Cache all ‘discovery information’ relating to a particular End Device.

The ZPS_tsAplZdpRemoveNodeCacheReqstructure is detailed below.

typedef struct { uint16 u16NwkAddr; uint64 u64IeeeAddr;
} ZPS_tsAplZdpRemoveNodeCacheReq;

where:

  • u16NwkAddris the network address of the End Device of interest

  • u64IeeeAddris the IEEE address of the End Device of interest

Parent topic:ZDP Request structures