ZPS_u64AplZdoLookupIeeeAddr
uint64 ZPS_u64AplZdoLookupIeeeAddr(
uint16 u16NwkAddr);
Description
This function can be used to search the local Address Map table for the 64-bit IEEE (MAC) address of the node with a given 16-bit network address.
Parent topic:ZPS_u64AplZdoLookupIeeeAddr
Parameters
u16NwkAddr 16-bit network address of node to be searched for.
Parent topic:ZPS_u64AplZdoLookupIeeeAddr
Returns
64-bit IEEE/MAC address obtained.
Parent topic:ZPS_u64AplZdoLookupIeeeAddr
Parent topic:Addressing functions