ZPS_u64GetFlashMappedIeeeAddress
uint64 ZPS_u64GetFlashMappedIeeeAddress(
uint16 u16Location);
Description
This function can be used on the Trust Centre to obtain the 64-bit IEEE (MAC) address of the node for which a link key has been persistently stored in the specified location in devices Flash memory. The location is specified as the number of the array element for the node - see the description of ZPS_vTcInitFlash.
Parent topic:ZPS_u64GetFlashMappedIeeeAddress
Parameters
u16Location: Number of the array element for the node
Parent topic:ZPS_u64GetFlashMappedIeeeAddress
Returns
64-bit IEEE/MAC address obtained.
Parent topic:ZPS_u64GetFlashMappedIeeeAddress
Parent topic:Addressing functions