ZPS_u64NwkNibGetEpid
uint64 ZPS_u64NwkNibGetEpid(void *pvNwk);
Description
This function can be used to obtain the Extended PAN ID (EPID) from a local NIB (Network Information Base).
The handle of the NWK layer instance that contains the relevant NIB must be specified. This handle can be obtained using ZPS_pvAplZdoGetNwkHandle().
Parent topic:ZPS_u64NwkNibGetEpid
Parameters
pNibHandle Pointer to NWK layer instance that contains the NIB
Parent topic:ZPS_u64NwkNibGetEpid
Returns
64-bit Extended PAN ID from NIB
Parent topic:ZPS_u64NwkNibGetEpid
Parent topic:Object Handle functions