ZPS_u8AplZdoGetRadioChannel
uint8 ZPS_u8AplZdoGetRadioChannel(void);
Description
This function obtains the 2400-MHz band channel in which the local node is currently operating. The channel is represented by an integer in the range 11 to 26.
Parent topic:ZPS_u8AplZdoGetRadioChannel
Parameters
None.
Parent topic:ZPS_u8AplZdoGetRadioChannel
Returns
Radio channel number (in range 11-26).
Parent topic:ZPS_u8AplZdoGetRadioChannel
Parent topic:Network deployment functions