ZPS_vNwkLinkCostCallbackRegister
void ZPS_vNwkLinkCostCallbackRegister(void *pvFn);
Description
This function can be used to register a user-defined callback function that defines custom mappings between LQI values and link costs that are to be used in packet filtering, based on link cost. When packet filtering is enabled, the stack uses a default set of mappings, detailed in Section 6.10.3.1. The callback function is only needed if custom mappings are to be used that will over-ride the default mappings. If required, this registration function must be called before ZPS_eAplAfInit(), and on both cold and warm starts.
The user-defined callback function to be registered has the following prototype:
uint8 APP_u8LinkCost(uint8 u8Lqi);
This callback function translates a measured LQI value (u8Lqi) into a link cost value. An example function is given in Section 6.10.3.3.
For more information on packet filtering and link costs, refer to Section 6.10.3.
Parent topic:ZPS_vNwkLinkCostCallbackRegister
Parameters
pvFn Pointer to user-defined callback function to be registered.
Parent topic:ZPS_vNwkLinkCostCallbackRegister
Returns
None.
Parent topic:ZPS_vNwkLinkCostCallbackRegister
Parent topic:initialization functions