ZPS_vNwkSendNwkStatusCommand
void ZPS_vNwkSendNwkStatusCommand(
void *pvNwk,
uint16 u16DstAddress,
uint16 u16TargetAddress,
uint8 u8CommandId,
uint8 u8Radius);
Description
This function can be used to send a network status command to another node. For example, it can be used by an End Device to report a routing problem (concerning a remote node) to its parent.
Parent topic:ZPS_vNwkSendNwkStatusCommand
Parameters
pvNwk Pointer to NWK layer instance
u16DstAddress Network address of the remote node to which the status command relates (for example, the node for which a routing problem is being reported)
u16TargetAddress Network address of the node to which the status command is to be sent (for example, the parent of the local node)
u8CommandId Value representing the network status command to be sent (the possible values are provided in the ZigBee PRO specification)
u8Radius Maximum number of hops permitted to target node (zero value specifies that default maximum is to be used)
Parent topic:ZPS_vNwkSendNwkStatusCommand
Returns
None
Parent topic:ZPS_vNwkSendNwkStatusCommand
Parent topic:Network deployment functions