ZQ_u32QueueGetQueueSize

bool_t ZQ_bQueueIsEmpty(void *pvQueueHandle);

Description

This function obtains the capacity of the specified message queue. The return code indicates the size of the queue in terms of the number of messages that it can hold.

Parent topic:ZQ_u32QueueGetQueueSize

Parameters

pvQueueHandle Handle of message queue

Parent topic:ZQ_u32QueueGetQueueSize

Returns

The capacity of the queue in terms of the number of messages that it can hold.

Parent topic:ZQ_u32QueueGetQueueSize

Parent topic:ZigBee queue functions