ZTIMER_eStop

ZTIMER_teStatus ZTIMER_eStop(uint8 u8TimerIndex);

Description

This function is used to stop the specified software timer (before it expires). The timer must have been previously started using ZTIMER_eStart().

Parent topic:ZTIMER_eStop

Parameters

pu8TimerIndex: Index number of the timer in the list of timers initialized using ZTIMER_eInit().

Parent topic:ZTIMER_eStop

Returns

  • E_ZTIMER_OK (timer successfully stopped)

  • E_ZTIMER_FAIL (timer not stopped - may be already stopped or expired)

Parent topic:ZTIMER_eStop

Parent topic:ZigBee Timer functions