Colour Dimmer Switch

The Colour Dimmer Switch device controls the hue, saturation and luminance of a multi-colour light, and to switch the light device on and off.

  • The Device ID is 0x0105.

  • The header file for the device is colour_dimmer_switch.h.

  • The clusters supported by the device are listed in Section 3.6.1.

  • The device structure, tsZLO_ColourDimmerSwitchDevice, is listed in Section 3.6.2.

  • The endpoint registration function for the device, eZLO_RegisterColourDimmerSwitchEndPoint(), is detailed in Section 3.6.3.

Supported clusters

The clusters used by the Colour Dimmer Switch device are listed in the table below.

Table 19.  Clusters for Colour Dimmer Switch

Server (input) side

Client (output) side

Mandatory

Basic

On/Off

Identify

Level control

Colour control

Identify

Optional

On/Off switch configuration

OTA upgrade

Scenes

Groups

The mandatory attributes within each cluster for this device type are indicated in the ZigBee Lighting and Occupancy Device Specification (15-0014-01).

Parent topic:Colour Dimmer Switch

Device Structure

The following tsZLO_ColourDimmerSwitchDevice structure is the shared structure for a Colour Dimmer Switch device:

typedef struct
{
    tsZCL_EndPointDefinition sEndPoint;
    /* Cluster instances */
    tsZLO_ColourDimmerSwitchDeviceClusterInstances sClusterInstance;
    /* Mandatory server clusters */
    #if (defined CLD_BASIC) && (defined BASIC_SERVER)
    /* Basic Cluster - Server */
    tsCLD_Basic sBasicServerCluster;
    #endif
    #if (defined CLD_IDENTIFY) && (defined IDENTIFY_SERVER)
    /* Identify Cluster - Server */
    tsCLD_Identify sIdentifyServerCluster;
    tsCLD_IdentifyCustomDataStructure
    sIdentifyServerCustomDataStructure;
    #endif
    /* Optional server clusters */
    #if (defined CLD_OOSC) && (defined OOSC_SERVER)
        /* On/Off Switch Configuration Cluster - Server */
        tsCLD_OOSC sOOSCServerCluster;
    #endif
    /* Mandatory client clusters */
    #if (defined CLD_IDENTIFY) && (defined IDENTIFY_CLIENT)
        /* Identify Cluster - Client */
        tsCLD_Identify sIdentifyClientCluster;
        tsCLD_IdentifyCustomDataStructure
        sIdentifyClientCustomDataStructure;
    #endif
    #if (defined CLD_BASIC) && (defined BASIC_CLIENT)
    /* Basic Cluster - Server */
        tsCLD_Basic sBasicClientCluster;
        #endif
    #if (defined CLD_ONOFF) && (defined ONOFF_CLIENT)
    tsCLD_OnOff sOnOffClientCluster;
    #endif
    #if (defined CLD_LEVEL_CONTROL) && (defined LEVEL_CONTROL_CLIENT)
    /* Level Control Cluster - Client */
        tsCLD_LevelControl sLevelControlClientCluster;
        tsCLD_LevelControlCustomDataStructure
        sLevelControlClientCustomDataStructure;
     #endif
    #if (defined CLD_COLOUR_CONTROL) && (defined COLOUR_CONTROL_CLIENT)
        /* Colour Control Cluster - Client */
        tsCLD_ColourControl sColourControlClientCluster;
        tsCLD_ColourControlCustomDataStructure
        sColourControlClientCustomDataStructure;
    #endif
    /*Recommended Optional client clusters */
    #if (defined CLD_SCENES) && (defined SCENES_CLIENT)
    /* Scenes Cluster - Client */
    tsCLD_Scenes sScenesClientCluster;
    tsCLD_ScenesCustomDataStructure sScenesClientCustomDataStructure;
    #endif
    #if (defined CLD_GROUPS) && (defined GROUPS_CLIENT)
    /* Groups Cluster - Client */
    tsCLD_Groups sGroupsClientCluster;
    tsCLD_GroupsCustomDataStructure sGroupsClientCustomDataStructure;
    #endif
    #if (defined CLD_OTA) && (defined OTA_CLIENT)
    tsCLD_AS_Ota sCLD_OTA;
    tsOTA_Common sCLD_OTA_CustomDataStruct;
    #endif
} tsZLO_ColourDimmerSwitchDevice;

Parent topic:Colour Dimmer Switch

Registration Function

The following eZLO_RegisterColourDimmerSwitchEndPoint() function is the endpoint registration function for a color Dimmer Switch device.

teZCL_Status eZLO_RegisterColourDimmerSwitchEndPoint(
                   uint8 u8EndPointIdentifier,
        tfpZCL_ZCLCallBackFunction cbCallBack,
             tsZLO_DimmerSwitchDevice *psDeviceInfo);

Description

This function is used to register an endpoint which supports a color Dimmer Switch device. The function must be called after eZCL_Initialise().

The specified identifier for the endpoint is a number in the range 1 to 240 (endpoint 0 is reserved for ZigBee use). Application endpoints are normally numbered consecutively starting at 1. The specified number must be less than or equal to the value of ZLO_NUMBER_OF_ENDPOINTS defined in the zcl_options.h file. This parameter represents the highest endpoint number used for applications.

While invoking this function, specify a user-defined callback function, which is invoked when an event associated with the endpoint occurs. This callback function is defined according to the typedef:

typedef void(* tfpZCL_ZCLCallBackFunction)
(tsZCL_CallBackEvent *pCallBackEvent);

You must also provide a pointer to a tsZLO_ColourDimmerSwitchDevice structure, described in Device Structure. This structure stores all variables relating to the color Controller device associated with the endpoint. This function sets the sEndPoint and sClusterInstance fields of this structure and these fields must not be directly written to by the application.

The function is called multiple times if more than one endpoint is being used - for example, if more than one color Dimmer Switch device is housed in the same hardware, sharing the same module.

Parameters

  • u8EndPointIdentifier: Endpoint that is to be associated with the registered structure and callback function.

  • cbCallBack: Pointer to the function that is used to indicate events to the application for this endpoint.

  • psDeviceInfo: Pointer to the structure that acts as storage for all variables related to the device being registered on this endpoint (see Device Structure). The sEndPoint and sClusterInstance fields are set by this register function for internal use and must not be written to by the application.

Returns

  1. E_ZCL_SUCCESS

  2. E_ZCL_FAIL

  3. E_ZCL_ERR_PARAMETER_NULL

  4. E_ZCL_ERR_PARAMETER_RANGE

  5. E_ZCL_ERR_EP_RANGE

  6. E_ZCL_ERR_CLUSTER_0

  7. E_ZCL_ERR_CALLBACK_NULL

  8. E_ZCL_ERR_CLUSTER_NULL

  9. E_ZCL_ERR_SECURITY_RANGE

  10. E_ZCL_ERR_CLUSTER_ID_RANGE

  11. E_ZCL_ERR_MANUFACTURER_SPECIFIC

  12. E_ZCL_ERR_ATTRIBUTE_TYPE_UNSUPPORTED

  13. E_ZCL_ERR_ATTRIBUTE_ID_ORDER

  14. E_ZCL_ERR_ATTRIBUTES_ACCESS

The above codes are described in the ZCL User Guide (JNUG3132).

Parent topic:Colour Dimmer Switch

Parent topic:Lighting and Occupancy Device Types