Device Structure

The following tsZLO_ColourDimmableLightDevice structure is the shared structure for a Colour Dimmable Light device:

typedef struct
{
    tsZCL_EndPointDefinition sEndPoint;
/* Cluster instances */
    tsZLO_DimmableLightDeviceClusterInstances sClusterInstance;
    #if (defined CLD_BASIC) && (defined BASIC_SERVER)
/* Basic Cluster - Server */
    tsCLD_Basic sBasicServerCluster;
    #endif
    #if (defined CLD_IDENTIFY) && (defined IDENTIFY_SERVER)
/* Identify Cluster - Server */
    tsCLD_Identify sIdentifyServerCluster;
    tsCLD_IdentifyCustomDataStructure
    sIdentifyServerCustomDataStructure;
    #endif
    #if (defined CLD_ONOFF) && (defined ONOFF_SERVER)
/* On/Off Cluster - Server */
    tsCLD_OnOff sOnOffServerCluster;
    tsCLD_OnOffCustomDataStructure sOnOffServerCustomDataStructure;
    #endif
    #if (defined CLD_GROUPS) && (defined GROUPS_SERVER)
/* Groups Cluster - Server */
    tsCLD_Groups sGroupsServerCluster;
    tsCLD_GroupsCustomDataStructure sGroupsServerCustomDataStructure;
    #endif
    #if (defined CLD_SCENES) && (defined SCENES_SERVER)
/* Scenes Cluster - Server */
    tsCLD_Scenes sScenesServerCluster;
    tsCLD_ScenesCustomDataStructure sScenesServerCustomDataStructure;
    #endif
    #if (defined CLD_LEVEL_CONTROL) && (defined LEVEL_CONTROL_SERVER)
/* LevelControl Cluster - Server */
    tsCLD_LevelControl sLevelControlServerCluster;
    tsCLD_LevelControlCustomDataStructure
    sLevelControlServerCustomDataStructure;
    #endif
    #if (defined CLD_ZLL_COMMISSION) && (defined ZLL_COMMISSION_SERVER)
    tsCLD_ZllCommission sZllCommissionServerCluster;
    tsCLD_ZllCommissionCustomDataStructure
    sZllCommissionServerCustomDataStructure;
    #endif
    #if (defined CLD_OTA) && (defined OTA_CLIENT)
/* OTA cluster - Client */
    tsCLD_AS_Ota sCLD_OTA;
    tsOTA_Common sCLD_OTA_CustomDataStruct;
    #endif
    #if (defined CLD_OCCUPANCY_SENSING) && (defined
OCCUPANCY_SENSING_CLIENT)
/* Occupancy Sensing Cluster - Client */
    tsCLD_OccupancySensing sOccupancySensingClientCluster;
    #endif
} tsZLO_DimmableLightDevice;

Parent topic:Colour Dimmable Light