Device Structure

The following tsZLO_OnOffPlugDevice structure is the shared structure for an On/Off Plug-in Unit device:

typedef struct
{
    tsZCL_EndPointDefinition sEndPoint;
  /* Cluster instances */
    tsZLO_OnOffPlugDeviceClusterInstances sClusterInstance;
  #if (defined CLD_BASIC) && (defined BASIC_SERVER)
    /* Basic Cluster - Server */
    tsCLD_Basic sBasicServerCluster;
  #endif
  #if (defined CLD_IDENTIFY) && (defined IDENTIFY_SERVER)
    /* Identify Cluster - Server */
    tsCLD_Identify sIdentifyServerCluster;
    tsCLD_IdentifyCustomDataStructure
        sIdentifyServerCustomDataStructure;
  #endif
  #if (defined CLD_ONOFF) && (defined ONOFF_SERVER)
    /* On/Off Cluster - Server */
    tsCLD_OnOff sOnOffServerCluster;
    tsCLD_OnOffCustomDataStructure
        sOnOffServerCustomDataStructure;
  #endif
  #if (defined CLD_GROUPS) && (defined GROUPS_SERVER)
  /* Groups Cluster - Server */
    tsCLD_Groups sGroupsServerCluster;
    tsCLD_GroupsCustomDataStructure
        sGroupsServerCustomDataStructure;
  #endif
  #if (defined CLD_SCENES) && (defined SCENES_SERVER)
    /* Scenes Cluster - Server */
    tsCLD_Scenes sScenesServerCluster;
    tsCLD_ScenesCustomDataStructure
        sScenesServerCustomDataStructure;
  #endif
  #if (defined CLD_LEVEL_CONTROL) && (defined LEVEL_CONTROL_SERVER)
    /* LevelControl Cluster - Server */
    tsCLD_LevelControl sLevelControlServerCluster;
    tsCLD_LevelControlCustomDataStructure
        sLevelControlServerCustomDataStructure;
  #endif
  #if (defined CLD_OTA) && (defined OTA_CLIENT)
    /* OTA cluster - Client */
    tsCLD_AS_Ota sCLD_OTA;
    tsOTA_Common sCLD_OTA_CustomDataStruct;
  #endif
} tsZLO_OnOffPlugDevice;

Parent topic:On/Off Plug-in Unit