Extended Colour Light

The Extended Colour Light device is typically used in nodes that contain a colour lamp with adjustable colour and brightness. This device supports a range of colour parameters, including hue/saturation, enhanced hue, colour temperature, colour loop, and XY.

  • The Device ID is 0x010D.

  • The header file for the device is extended_colour_light.h.

  • The clusters supported by the device are listed in Section 3.14.1.

  • The device structure, tsZLO_ExtendedColourLightDevice, is listed in Section 3.14.2.

  • The endpoint registration function for the device, eZLO_RegisterExtendedColourLightEndPoint(), is detailed in Section 3.14.3.

Supported clusters

The clusters supported by the Extended Colour Light device are listed in the table below.

Table 27.  Clusters for Extended Colour Light

Server (Input) side

Client (Output) side

Mandatory

Basic

Identify

Groups

Scenes

On/Off

Level control

Colour control

Optional

Touchlink commissioning

OTA upgrade

The mandatory attributes within each cluster for this device type are indicated in the ZigBee Lighting and Occupancy Device Specification (15-0014-01).

Parent topic:Extended Colour Light

Device Structure

The following tsZLO_ExtendedColourLightDevice structure is the shared structure for an Extended color Light device:

typedef struct
{
  tsZCL_EndPointDefinition sEndPoint;
  /*Clusterinstances*/
    tsZLO_ExtendedColourLightDeviceClusterInstances
                                  sClusterInstance;
  #if (defined CLD_BASIC) && (defined BASIC_SERVER)
    /* Basic Cluster - Server */
    tsCLD_Basic sBasicServerCluster;
  #endif
  #if (defined CLD_IDENTIFY) && (defined IDENTIFY_SERVER)
    /* Identify Cluster - Server */
    tsCLD_Identify sIdentifyServerCluster;
    tsCLD_IdentifyCustomDataStructure
            sIdentifyServerCustomDataStructure;
  #endif
  #if (defined CLD_ONOFF) && (defined ONOFF_SERVER)
    /* On/Off Cluster - Server */
    tsCLD_OnOff sOnOffServerCluster;
    tsCLD_OnOffCustomDataStructure sOnOffServerCustomDataStructure;
  #endif
  #if (defined CLD_GROUPS) && (defined GROUPS_SERVER)
    /* Groups Cluster - Server */
    tsCLD_Groups sGroupsServerCluster;
    tsCLD_GroupsCustomDataStructure sGroupsServerCustomDataStructure;
    #endif
  #if (defined CLD_SCENES) && (defined SCENES_SERVER)
    /* Scenes Cluster - Server */
    tsCLD_Scenes sScenesServerCluster;
    tsCLD_ScenesCustomDataStructure sScenesServerCustomDataStructure;
  #endif
  #if (defined CLD_LEVEL_CONTROL) && (defined LEVEL_CONTROL_SERVER)
    /* LevelControl Cluster - Server */
    tsCLD_LevelControl sLevelControlServerCluster;
    tsCLD_LevelControlCustomDataStructure
    sLevelControlServerCustomDataStructure;
  #endif
  #if (defined CLD_COLOUR_CONTROL) && (defined COLOUR_CONTROL_SERVER)
    /* Colour Control Cluster - Server */
    tsCLD_ColourControl sColourControlServerCluster;
    tsCLD_ColourControlCustomDataStructure
    sColourControlServerCustomDataStructure;
  #endif
  #if (defined CLD_ZLL_COMMISSION) && (defined ZLL_COMMISSION_SERVER)
    tsCLD_ZllCommission sZllCommissionServerCluster;
    tsCLD_ZllCommissionCustomDataStructure
    sZllCommissionServerCustomDataStructure;
  #endif
  #if (defined CLD_OTA) && (defined OTA_CLIENT)
    /* OTA cluster - Client */
    tsCLD_AS_Ota sCLD_OTA;
    tsOTA_Common sCLD_OTA_CustomDataStruct;
    #endif
} tsZLO_ExtendedColourLightDevice;

Parent topic:Extended Colour Light

Registration Function

The following eZLO_RegisterExtendedColourLightEndPoint() function is the endpoint registration function for an Extended color Light device.

teZCL_Status eZLO_RegisterExtendedColourLightEndPoint(
uint8 u8EndPointIdentifier,
tfpZCL_ZCLCallBackFunction cbCallBack,
tsZLO_ExtendedColourLightDevice *psDeviceInfo);

Description

This function is used to register an endpoint which supports an Extended color Light device. The function must be called after eZCL_Initialise().

The specified identifier for the endpoint is a number in the range 1 to 240 (endpoint 0 is reserved for ZigBee use). Application endpoints are normally numbered consecutively starting at 1. The specified number must be less than or equal to the value of ZLO_NUMBER_OF_ENDPOINTS defined in the zcl_options.h file, which represents the highest endpoint number used for applications.

While invoking this function, specify a user-defined callback function, which is invoked when an event associated with the endpoint occurs. This callback function is defined according to the typedef:

typedef void(* tfpZCL_ZCLCallBackFunction)
(tsZCL_CallBackEvent *pCallBackEvent);

Also provide a pointer to a tsZLO_ExtendedColourLightDevice structure, described in Section 3.14.2. This structure stores all variables relating to the color Controller device associated with the endpoint. The sEndPoint and sClusterInstance fields of this structure are set by this function and must not be directly written to by the application.

The function is called multiple times if more than one endpoint is being used - for example, if more than one Extended color Light device is housed in the same hardware, sharing the same module.

Parameters

  • u8EndPointIdentifier: Endpoint that is to be associated with the registered structure and callback function.

  • cbCallBack: Pointer to the function that is used to indicate events to the application for this endpoint.

  • psDeviceInfo: Pointer to the structure that acts as storage for all variables related to the device being registered on this endpoint (see Section 3.14.2). The sEndPoint and sClusterInstance fields are set by this register function for internal use and must not be written to by the application.

Returns

  1. E_ZCL_SUCCESS

  2. E_ZCL_FAIL

  3. E_ZCL_ERR_PARAMETER_NULL

  4. E_ZCL_ERR_PARAMETER_RANGE

  5. E_ZCL_ERR_EP_RANGE

  6. E_ZCL_ERR_CLUSTER_0

  7. E_ZCL_ERR_CALLBACK_NULL

  8. E_ZCL_ERR_CLUSTER_NULL

  9. E_ZCL_ERR_SECURITY_RANGE

  10. E_ZCL_ERR_CLUSTER_ID_RANGE

  11. E_ZCL_ERR_MANUFACTURER_SPECIFIC

  12. E_ZCL_ERR_ATTRIBUTE_TYPE_UNSUPPORTED

  13. E_ZCL_ERR_ATTRIBUTE_ID_ORDER

  14. E_ZCL_ERR_ATTRIBUTES_ACCESS

The above codes are described in the ZCL User Guide (JNUG3132).

Parent topic:Extended Colour Light

Parent topic:Lighting and Occupancy Device Types