Initializing and starting the ZigBee Base Device
Initialize the ZigBee Base Device in the application code using the function BDB_vInit(). Call this function after initializing the ZigBee PRO stack and after restoring the ZigBee Base Device attribute bbdbNodeIsOnANetwork from persistent storage.
Note:
BDB_vInit() internally calls the function BDB_vSetKeys(), which loads into memory the pre-configured link key from the file bdb_link_keys.c. Network security and the pre-configured link keys are described in Section 2.3.
The ZigBee Base Device requires a number of internal software times, the number defined by the macro BDB_ZTIMER_STORAGE. Therefore, when the application calls ZTIMER_eInit() to initialize the required software timers and allocate storage (array elements) for them, it must add BDB_ZTIMER_STORAGE timers for use by the ZigBee Base Device. This function must be called before BDB_vInit(). Software timers and their associated functions are described in the ZigBee 3.0 Stack User Guide (JNUG3130).
The ZigBee Base Device is started by calling the function BDB_vStart(). This function may or may not perform an action. It depends on the node type and whether the node was previously a member of a network. In both cases, the function finally invokes the callback function APP_vBdbCallback() with a suitable event.
If the node was not on a network:
For a Router node that supports Touchlink commissioning (see Touchlink), the function selects a radio channel for the node from the set of primary channels for Touchlink specified in the BDBC_TL_PRIMARY_CHANNEL_SET bitmap (see Touchlink constants). Either the first channel of the specified set selects or, if the macro RAND_CHANNEL is set to TRUE (in the file bdb_options.h), a channel selects from the set at random.
For the Coordinator and other Router and End Device nodes, no action is taken. The application must then form a network (Coordinator or Router). Alternatively, it can join the node to a network using one of the commissioning methods described in Network commissioning (End Device or Router).
In the above cases, the function generates a BDB_EVENT_INIT_SUCCESS
event.
If the node was on a network:
For Coordinator and Router nodes, no action is taken and the function generates a BDB_EVENT_INIT_SUCCESS
event.
For an End Device node, the function attempts to rejoin the node to the network. It performs a series of rejoin cycles, where each cycle comprises the following three rejoin attempts:
First attempt with the previously used network parameters (without network discovery)
Second attempt with network discovery on the set of primary channels specified in the u32bdbPrimaryChannelSet bitmap (attribute)
Third attempt with network discovery on the set of secondary channels specified in the u32bdbSecondaryChannelSet bitmap (attribute)
The channel bitmaps are ZigBee Base Device attributes, described in Section 2.5.1.
The above rejoin cycle performs up to a maximum of BDBC_IMP_MAX_REJOIN_CYCLES times, which is an implementation-specific ZigBee Base Device constant (see Section 2.5.2).
If a rejoin attempt is successful, the function generates the event BDB_EVENT_REJOIN_SUCCESS.
If all the rejoin attempts are unsuccessful, the function generates the event BDB_EVENT_REJOIN_FAILURE unless unsecured joins are enabled through the APS attribute apsUseInsecureJoin, in which case the function attempts a join through Network Steering (described in Network steering). The nature of the join depends on the value of the Extended PAN ID (EPID) set in the APS attribute ApsUseExtendedPanid:
For a non-zero EPID, the node attempts to join the network with this EPID.
For a zero EPID, the function attempts to join any available network.
This join is attempted with an automatic call to the functionBDB_eNsStartNwkSteering().
Parent topic:ZigBee Base Device