On/Off Sensor

The On/Off Sensor device is used in sensor nodes that issue control commands, for example, an infrared occupancy sensor.

  • The Device ID is 0x0850.

  • The header file for the device is on_off_sensor.h.

  • The clusters supported by the device are listed in Supported clusters.

  • The device structure, tsZLO_OnOffSensorDevice, is listed in Device structure.

  • The endpoint registration function for the device, eZLO_RegisterOnOffSensorEndPoint(), is detailed in Registration function.

Supported clusters

The clusters used by the On/Off Sensor device are listed in the table below.

Table 34.  Clusters for On/Off Sensor

Server (Input) side

Client (Output) side

Mandatory

Basic

On/Off

Identify

Identify

Optional

Touchlink commissioning

Touchlink commissioning

Level control

Colour control

Groups

Scenes

OTA upgrade

The mandatory attributes within each cluster for this device type are indicated in the ZigBee Lighting and Occupancy Device Specification (15-0014-01).

Parent topic:On/Off Sensor

Device structure

The following tsZLO_OnOffSensorDevice structure is the shared structure for a On/Off Sensor device:

typedef struct
{
  tsZCL_EndPointDefinition sEndPoint;
  /* Cluster instances */
  tsZLO_OnOffSensorDeviceClusterInstances sClusterInstance;
  #if (defined CLD_BASIC) && (defined BASIC_SERVER)
    /* Basic Cluster - Server */
    tsCLD_Basic sBasicServerCluster;
  #endif
  #if (defined CLD_IDENTIFY) && (defined IDENTIFY_SERVER)
    /* Identify Cluster - Server */
    tsCLD_Identify sIdentifyServerCluster;
    tsCLD_IdentifyCustomDataStructure
          sIdentifyServerCustomDataStructure;
    #endif
  /* Recommended Optional Server Cluster */
  #if (defined CLD_ZLL_COMMISSION) && (defined ZLL_COMMISSION_SERVER)
    tsCLD_ZllCommission sZllCommissionServerCluster;
    tsCLD_ZllCommissionCustomDataStructure
          sZllCommissionServerCustomDataStructure;
  #endif
/** Mandatory client clusters*/
  #if (defined CLD_IDENTIFY) && (defined IDENTIFY_CLIENT)
    /* Identify Cluster - Client */
    tsCLD_Identify sIdentifyClientCluster;
    tsCLD_IdentifyCustomDataStructure
          sIdentifyClientCustomDataStructure;
  #endif
  #if (defined CLD_ONOFF) && (defined ONOFF_CLIENT)
  /* On/Off Cluster - Client */
  tsCLD_OnOff sOnOffClientCluster;
  #endif
  /* Recommended Optional Client CLuster */
  #if (defined CLD_LEVEL_CONTROL) && (defined LEVEL_CONTROL_CLIENT)
    /* Level Control Cluster - Client */
    tsCLD_LevelControl sLevelControlClientCluster;
    tsCLD_LevelControlCustomDataStructure
          sLevelControlClientCustomDataStructure;
  #endif
  #if (defined CLD_SCENES) && (defined SCENES_CLIENT)
  /* Scenes Cluster - Client */
  tsCLD_Scenes sScenesClientCluster;
  tsCLD_ScenesCustomDataStructure sScenesClientCustomDataStructure;
  #endif
  #if (defined CLD_GROUPS) && (defined GROUPS_CLIENT)
    /* Groups Cluster - Client */
    tsCLD_Groups sGroupsClientCluster;
    tsCLD_GroupsCustomDataStructure sGroupsClientCustomDataStructure;
  #endif
  #if (defined CLD_COLOUR_CONTROL) && (defined COLOUR_CONTROL_CLIENT)
    /* Colour Control Cluster - Client */
    tsCLD_ColourControl sColourControlClientCluster;
    tsCLD_ColourControlCustomDataStructure
            sColourControlClientCustomDataStructure;
  #endif
  #if (defined CLD_OTA) && (defined OTA_CLIENT)
    /* OTA cluster - Client */
    tsCLD_AS_Ota sCLD_OTA;
    tsOTA_Common sCLD_OTA_CustomDataStruct;
  #endif
  #if (defined CLD_ZLL_COMMISSION) && (defined ZLL_COMMISSION_CLIENT)
  tsCLD_ZllCommission sZllCommissionClientCluster;
  tsCLD_ZllCommissionCustomDataStructure
          sZllCommissionClientCustomDataStructure;
  #endif
} tsZLO_OnOffSensorDevice;

Parent topic:On/Off Sensor

Registration function

The following eZLO_RegisterOnOffSensorEndPoint() function is the endpoint registration function for an On/Off Sensor device.

teZCL_Status eZLO_RegisterOnOffSensorEndPoint(
uint8 *u8EndPointIdentifier,
tfpZCL_ZCLCallBackFunction cbCallBack,
tsZLO_OnOffSensorDevice *psDeviceInfo);

Description

This function is used to register an endpoint which supports an On/Off Sensor device. The function must be called after eZCL_Initialise().

The specified identifier for the endpoint is a number in the range 1 to 240 (endpoint 0 is reserved for ZigBee use). Application endpoints are normally numbered consecutively starting at 1. The specified number must be less than or equal to the value of ZLO_NUMBER_OF_ENDPOINTS defined in the zcl_options.h file, which represents the highest endpoint number used for applications.

While invoking this function, specify a user-defined callback function, which is invoked when an event associated with the endpoint occurs. This callback function is defined according to the typedef:

typedef void(* tfpZCL_ZCLCallBackFunction)
(tsZCL_CallBackEvent *pCallBackEvent);

Also provide a pointer to a tsZLO_OnOffSensorDevice structure, described in Device structure. This structure stores all variables relating to the color Controller device associated with the endpoint. The sEndPoint and sClusterInstance fields of this structure are set by this function and must not be directly written to by the application.

The function is called multiple times if more than one endpoint is being used - for example, if more than one On/Off Sensor device is housed in the same hardware, sharing the same module.

Parameters

  • u8EndPointIdentifier: Endpoint that is to be associated with the registered structure and callback function.

  • cbCallBack: Pointer to the function that is used to indicate events to the application for this endpoint.

  • psDeviceInfo: Pointer to the structure that acts as storage for all variables related to the device being registered on this endpoint (see Device structure). The sEndPoint and sClusterInstance fields are set by this register function for internal use and must not be written to by the application.

Returns

  1. E_ZCL_SUCCESS

  2. E_ZCL_FAIL

  3. E_ZCL_ERR_PARAMETER_NULL

  4. E_ZCL_ERR_PARAMETER_RANGE

  5. E_ZCL_ERR_EP_RANGE

  6. E_ZCL_ERR_CLUSTER_0

  7. E_ZCL_ERR_CALLBACK_NULL

  8. E_ZCL_ERR_CLUSTER_NULL

  9. E_ZCL_ERR_SECURITY_RANGE

  10. E_ZCL_ERR_CLUSTER_ID_RANGE

  11. E_ZCL_ERR_MANUFACTURER_SPECIFIC

  12. E_ZCL_ERR_ATTRIBUTE_TYPE_UNSUPPORTED

  13. E_ZCL_ERR_ATTRIBUTE_ID_ORDER

  14. E_ZCL_ERR_ATTRIBUTES_ACCESS

The above codes are described in the ZCL User Guide (JNUG3132).

Parent topic:On/Off Sensor

Parent topic:Lighting and Occupancy Device Types