Overview

This manual describes ZigBee 3.0 software architecture and the supported Zigbee device types. It also describes Zigbee Lighting and Occupancy device types and how to implement these devices on the FRDM-MCXW71, FRDM-MCXW72, MCX-W71-EVK, MCX-W72-EVK, FRDM-RW612 board, and RD-RW612-BGA hardware platforms provided by NXP. These platforms belong to the NXP provided MCXW71, MCXW72 and RW612 family of wireless microcontrollers.

The device software described in this manual can be used on the NXP MCXW71, MCXW72 and RW612 family of wireless microcontrollers.

The document is organized as follows:

Conventions

  • Bold type font represents Files, folders, GUI elements, function names, and parameter types.

  • italics type font represents function parameters.

  • Courier New typeface represents Code fragments.

    Note: This is a sample Note. It highlights important additional information.

Parent topic:Overview

Acronyms and abbreviations

Table 1 lists the acronyms and abbreviations used in this document.

Acronym

Description

ACE

Ancillary Control Equipment

APDU

Application Protocol Data Unit

API

Application Programming Interface

BDB

Base Device Behavior

CIE

Control and Indicating Equipment

DRLC

Demand-Response and Load Control

HA

Home Automation

IAS

Intruder Alarm System

SDK

Software Development Kit

SE

Smart Energy

WD

Warning Device

ZBD

ZigBee Base Device

ZCL

ZigBee Cluster Library

ZLO

ZigBee Lighting and Occupancy

ZPS

ZigBee PRO Stack

Parent topic:Overview