Alarm Notification Payload

typedef struct
{
  uint8   u8AlarmCode;
  uint16   u16ClusterId;
} tsCLD_AlarmsAlarmCommandPayload;

where:

  • u8AlarmCode is the code which identifies the type of alarm that has been generated - these codes are cluster-specific

  • u16ClusterId is the Cluster ID of the cluster which generated the alarm

Parent topic:Custom Command Payloads