eCLD_AlarmsResetAlarmLog
teZCL_Status eCLD_AlarmsResetAlarmLog(
tsZCL_EndPointDefinition *psEndPointDefinition,
tsZCL_ClusterInstance *psClusterInstance);
Description
This function can be called on the Alarms cluster server to clear all entries of the local Alarms table. The function may be called as the result of user input.
Parameters
psEndPointDefinition: Pointer to the ZCL endpoint definition structure for the application (see Section 6.1.1)
psClusterInstance: Pointer to structure containing information about the Alarms cluster instance (see Section 6.1.16)
Returns
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().
Parent topic:Functions