Functions
The following Diagnostics cluster functions are provided:
The cluster attributes can also all be accessed using the general attribute read/write functions, as described in Section 2.3.
eCLD_DiagnosticsCreateDiagnostics
teZCL_Status eCLD_DiagnosticsCreateDiagnostics(
tsZCL_ClusterInstance *psClusterInstance,
bool_t bIsServer,
tsZCL_ClusterDefinition *psClusterDefinition,
void *pvEndPointSharedStructPtr,
uint8 *pu8AttributeControlBits);
Description
This function creates an instance of the Diagnostics cluster on an endpoint. The cluster instance is created on the endpoint which is associated with the supplied tsZCL_ClusterInstance
structure and can act as a server or a client, as specified.
The function should only be called when setting up a custom endpoint containing one or more selected clusters (rather than the whole set of clusters supported by a standard ZigBee device). This function creates a Diagnostics cluster instance on the endpoint, but instances of other clusters may also be created on the same endpoint by calling their corresponding creation functions.
Note: This function must not be called for an endpoint on which a standard ZigBee device is used. In this case, the device and its supported clusters must be registered on the endpoint using the relevant device registration function.
When used, this function must be called after the stack has been started and after the ZCL has been initialized.
Parameters
psClusterInstance: Pointer to structure containing information about the cluster instance to be created (see Section 6.1.16). This structure is updated by the function by initializing individual structure fields.
bIsServer: Type of cluster instance (server or client) to be created:
TRUE - server
FALSE - client
psClusterDefinition: Pointer to structure indicating the type of cluster to be created (see Section 6.1.2). In this case, this structure must contain the details of the Diagnostics cluster. This parameter can refer to a pre-filled structure called
sCLD_Diagnostics
which is provided in the Diagnostics.h file.pvEndPointSharedStructPtr: Pointer to the shared structure used for attribute storage. This parameter should be the address of the structure of type
tsCLD_Diagnostics
which defines the attributes of Diagnostics cluster. The function initializes the attributes with default values.pu8AttributeControlBits: Pointer to an array of uint8 values, with one element for each attribute in the cluster (see above).
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_INVALID_VALUE
Parent topic:Functions
eCLD_DiagnosticsUpdate
teZCL_Status eCLD_DiagnosticsUpdate(
uint8 u8SourceEndPointId);
Description
This function updates the (three) Stack/Network Information attributes (see Section22.2). It should be called periodically by the application (on the cluster server) at the highest rate possible or when an appropriate stack event occurs.
The attributes can otherwise be accessed (for example, read) using the Attribute Access functions detailed in Section 5.2.
Parameters
u8SourceEndPointId: Number of the local endpoint on which cluster server resides
Returns
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
Parent topic:Functions
Parent topic:Diagnostics Cluster