eCLD_GroupsCommandAddGroupIfIdentifyingRequestSend

teZCL_Status eCLD_GroupsCommandAddGroupIfIdentifyingRequestSend
    (uint8 u8SourceEndPointId,
    uint8 u8DestinationEndPointId,
    tsZCL_Address *psDestinationAddress,
    uint8 *pu8TransactionSequenceNumber,
    tsCLD_Groups_AddGroupRequestPayload
    *psPayload);

Description

This function sends an Add Group If Identifying command to a remote device, requesting that the specified endpoints on the target device be added to a particular group on the condition that the remote device is identifying itself. The group ID/address and name (if supported) are specified in the payload of the message, and must be added to the Group table on the target node along with the associated endpoint numbers. The identifying functionality is controlled using the Identify cluster (see Chapter 11).

The device receiving this message generates a callback event on the endpoint on which the Groups cluster is registered and then checks whether the device is identifying itself. If so, the device (if possible) adds the group ID and group name to its Group table. If the device is not identifying itself, then no action is taken.

You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.

Parameters

  • u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.

  • u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP.

  • psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.

  • pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.

  • psPayload: Pointer to a structure containing the payload for this message (see Section 12.6.3).

Returns

  • E_ZCL_SUCCESS

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_EP_RANGE

  • E_ZCL_ERR_EP_UNKNOWN

  • E_ZCL_ERR_CLUSTER_NOT_FOUND

  • E_ZCL_ERR_ZBUFFER_FAIL

  • E_ZCL_ERR_ZTRANSMIT_FAIL

If an error is returned by the ZigBee PRO stack function, which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().

Parent topic:Functions