Initialization
The function eCLD_GroupsCreateGroups() is used to create an instance of the Groups cluster. The function is called by the initialization function for the host device.
A local endpoint can be added to a group on the local node using the function eCLD_GroupsAdd(). If the group does not exist, the function creates it. Therefore, this is a way of creating a local group.
Parent topic:Groups Cluster