eCLD_IdentifyCommandIdentifyQueryRequestSend
tsZCL_Status eCLD_IdentifyCommandIdentifyQueryRequestSend(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
uint8 *pu8TransactionSequenceNumber);
Description
This function can be called on a client device to send a custom command requesting a response from any server devices that are currently in identification mode.
A device which receives this command generates a callback event on the endpoint on which the Identify cluster is registered. If the receiving device is in identification mode, it returns a response containing the amount of time for which it continues in this mode (see Section 11.7.3).
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters
u8SourceEndPointId: Number of the local endpoint through which to send the request. This parameter is used both to send the message and to identify the instance of the shared structure holding the required attribute values.
u8DestinationEndPointId: Number of the endpoint on the remote node to which the request is sent. This parameter is ignored when sending to address types eZCL_AMBOUND and eZCL_AMGROUP.
psDestinationAddress: Pointer to a structure holding the address of the node to which the request is sent.
pu8TransactionSequenceNumber: Pointer to a location to receive the Transaction Sequence Number (TSN) of the request.
Returns
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_EP_UNKNOWN
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_ZCL_ERR_ZBUFFER_FAIL
E_ZCL_ERR_ZTRANSMIT_FAIL
If an error is returned by the ZigBee PRO stack function which is invoked by this function to transmit the data, this error may be obtained by calling eZCL_GetLastZpsError().
Parent topic:Functions