Compile-time options

  • To enable the On/Off cluster in the code to be built, it is necessary to add the following to the zcl_options.h file:

    #define CLD_ONOFF
    
    
  • In addition, to include the software for a cluster client or server or both, it is necessary to add one or both of the following to the same file:

    #define ONOFF_CLIENT
    #define ONOFF_SERVER
    
    
  • The On/Off cluster contains macros that may be optionally specified at compile time by adding some or all of the following lines to the zcl_options.h file.

Optional Attributes

  1. To enable the optional On Configurable Duration attribute, add this line:

    #define CLD_ONOFF_ATTR_ID_ON_CONFIGURABLE_DURATION
    
  2. To enable the optional Duration Unit of Measure attribute, add this line:

    #define CLD_ONOFF_ATTR_ID_DURATION_UNIT_OF_MEASUREMENT
    
    
  3. To enable the optional Maximum Duration attribute, add this line:

    #define CLD_ONOFF_ATTR_ID_MAX_DURATION
    
    
  4. To enable the optional Global Scene Control attribute, add this line:

    #define CLD_ONOFF_ATTR_GLOBAL_SCENE_CONTROL
    
    
  5. To enable the optional On Time attribute, add this line:

    #define CLD_ONOFF_ATTR_ON_TIME
    
    
  6. To enable the optional Off Wait Time attribute, add this line:

    #define CLD_ONOFF_ATTR_OFF_WAIT_TIME
    
    
  7. To enable the optional Start-up On/Off attribute, add this line:

    #define CLD_ONOFF_ATTR_STARTUP_ONOFF
    
    
  8. To enable the optional Attribute Reporting Status attribute, add this line:

    #define CLD_ONOFF_ATTR_ID_ATTRIBUTE_REPORTING_STATUS
    
    

Optional Commands

  1. Add this line to enable processing of the On With Recall Global Scene command on the server:

    #define CLD_ONOFF_CMD_ON_WITH_RECALL_GLOBAL_SCENE
    
  2. Add this line to enable the optional On With Timed Off command on the client and server:

    #define CLD_ONOFF_CMD_ON_WITH_TIMED_OFF
    
  3. Add this line to enable the optional Off With Effect command on the client and server:

    #define CLD_ONOFF_CMD_OFF_WITH_EFFECT
    

Cluster Revision

To define the value (n) of the Cluster Revision attribute, add this line:

#define CLD_ONOFF_CLUSTER_REVISION <n>

The default value is 1, which corresponds to the revision of the cluster in the ZCL r6 specification (see Section 2.4).

Parent topic:On/Off Cluster