eSE_PriceAddCalorificValueEntry
teZCL_Status eSE_PriceAddCalorificValueEntry(
uint8 u8SourceEndPointId,
uint8 u8DestinationEndPointId,
tsZCL_Address *psDestinationAddress,
bool_t bOverwritePrevious,
tsSE_PricePublishCalorificValueCmdPayload
*psPublishCalorificValueCmdPayload,
uint8 *pu8TransactionSequenceNumber);
Description
The function can be used on a Price cluster server to add a calorific value entry to the internal list of scheduled calorific values maintained by the cluster. The function also sends an unsolicited Publish Calorific Value command to the Price cluster client nodes in the network, to advertise the new calorific value. Therefore, the function should be called on the ESP when a new calorific value is received from the utility company.
On receiving the Publish Calorific Value command, a remote client automatically adds the new calorific value to the local calorific value list. However, if the new entry has the same start-time as an existing entry in the list, the outcome depends on the setting of the boolean parameter bOverwritePrevious in this function:
If this parameter is set to TRUE then the existing entry is removed and the new entry is added
If this parameter is set to FALSE then the Issuer Event IDs of the two calorific value entries are compared:
If the Event ID of the new entry is the greater, the existing entry is removed and the new entry is added
If the Event ID of the existing entry is the greater, E_ZCL_FAIL is returned and the list is not modified
A pointer must be specified to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request.
Parameters
u8SourceEndPointId: Number of the local endpoint through which the request is sent
u8DestinationEndPointId: Number of the remote endpoint to which the request is sent
psDestinationAddress: Pointer to a structure containing the address of the remote node to which the request is sent
bOverwritePrevious: Determines whether an existing calorific value with the same start-time on the clients will be over-written without comparing Event IDs (see above):
TRUE - over-write existing entry
FALSE - compare Event IDs first
psPublishCalorificValueCmdPayload Pointer to calorific value entry to be added to list on server and advertised to clients
pu8TransactionSequenceNumber Pointer to a location to store the Transaction Sequence Number (TSN) of the request
Returns
E_ZCL_SUCCESS
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_TIME_NOT_SYNCHRONISED
Parent topic:Functions