eSE_PriceDoesConversionFactorEntryExist
teSE_PriceStatus eSE_PriceDoesConversionFactorEntryExist(
uint8 u8SourceEndPointId,
bool_t bIsServer,
uint32 u32StartTime);
Description
This function can be used to check whether a conversion factor entry with the specified start-time is present in a conversion factor list on the local device.
You must specify the endpoint on which the local Price cluster resides and whether this cluster instance is a server or a client.
For a conversion factor entry to be successfully found, the specified start-time must exactly match the start-time of an entry in the conversion factor list, otherwise the status code E_SE_PRICE_NOT_FOUND will be returned.
Parameters
u8SourceEndPointId Number of the local endpoint for the conversion factor list to be accessed
bIsServer Nature of the Price cluster instance containing the price list:
TRUE - server
FALSE - client
u32StartTime Start-time of the conversion factor entry to search for
Returns
E_ZCL_SUCCESS
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_SE_PRICE_NOT_FOUND
Parent topic:Functions