eSE_PriceRemovePriceEntry
teSE_PriceStatus eSE_PriceRemovePriceEntry(
uint8 u8SourceEndPointId,
bool_t bIsServer,
uint32 u32StartTime);
Description
This function can be used to delete a price entry with specified start-time from a price list on the local device.
You must specify the endpoint on which the local Price cluster resides and whether this cluster instance is a server or a client.
For the successful deletion of a price entry, the specified start-time must exactly match the start-time of an entry in the price list, otherwise the status code E_SE_PRICE_NOT_FOUND will be returned.
Parameters
u8SourceEndPointId Number of the local endpoint on which Price cluster resides
bIsServer Nature of the Price cluster instance containing the price list:
TRUE - server
FALSE - client
u32StartTime The start-time of the price entry to delete
Returns
E_ZCL_SUCCESS
E_ZCL_ERR_CLUSTER_NOT_FOUND
E_SE_PRICE_NOT_FOUND
E_SE_PRICE_TABLE_NOT_FOUND
Parent topic:Functions