Compile-time options
To enable the Scenes cluster in the code to be built, it is necessary to add the following to the zcl_options.h file:
#define CLD_SCENES
In addition, to include the software for a cluster client or server or both, it is necessary to add one or both of the following to the same file:
#define SCENES_CLIENT
#define SCENES_SERVER
The Scenes cluster contains macros that may be optionally specified at compile time by adding some or all the following lines to the zcl_options.h file.
To enable the optional Last Configured By attribute, add this line:
#define CLD_SCENES_ATTR_LAST_CONFIGURED_BY
To configure the maximum length of the Scene Name storage, add this line:
#define CLD_SCENES_MAX_SCENE_NAME_LENGTH (16)
To configure the maximum number of scenes, add this line:
#define CLD_SCENES_MAX_NUMBER_OF_SCENES (16)
To configure the maximum number of bytes available for scene storage, add this line:
#define CLD_SCENES_MAX_SCENE_STORAGE_BYTES (20)
To enable the Enhanced Add Scene command, add this line:
#define CLD_SCENES_CMD_ENHANCED_ADD_SCENE
To enable the Enhanced View Scene command, add this line:
#define CLD_SCENES_CMD_ENHANCED_VIEW_SCENE
To enable the Copy Scene command, add this line:
#define CLD_SCENES_CMD_COPY_SCENE
To enable TransitionTime100ms in Scene tables, add this line:
#define CLD_SCENES_TABLE_SUPPORT_TRANSITION_TIME_IN_MS
To define the value (n) of the Cluster Revision attribute, add this line:
#define CLD_SCENES_CLUSTER_REVISION <n>
The default value is 1, which corresponds to the revision of the cluster in the ZCL r6 specification (see Section 2.4).
Parent topic:Scenes Cluster