Processing Events
This section outlines how the application should deal with stack events and timer events that are generated externally to the ZCL. A cluster-specific event initially arrives as one of these events.
The occurrence of an event in the ZCL queue activates a ZCL user function. The following actions must then be performed in the application:
The task checks whether the event that has occurred is a timer event (timer messages are collected by a user-defined function).
The task sets fields of the event structure
tsZCL_CallBackEvent
(see Section 3.1), as follows (all other fields are ignored):
For a timer event, sets the field
eEventType
to E_ZCL_CBET_TIMER.For a millisecond timer event, sets the field
eEventType
to E_ZCL_CBET_TIMER_MS.For a stack event, sets the field
eEventType
to E_ZCL_ZIGBEE_EVENT and sets the fieldpZPSevent
to point to theZPS_tsAfEvent
structure received by the application. This structure is defined in the ZigBee 3.0 Stack User Guide (JNUG3130).
The task passes this event structure to the ZCL using vZCL_EventHandler() - the ZCL then identifies the event type (see Section 3.3) and invokes the appropriate endpoint callback function.
Note: For a cluster-specific event (which arrives as a stack event or a timer event), the cluster normally contains its own event handler which is invoked by the ZCL. If the event requires the attention of the application, the ZCL replaces the eEventType
field with E_ZCL_CBET_CLUSTER_CUSTOM and populates the tsZCL_ClusterCustomMessage
structure with the event data. The ZCL then invokes the user-defined endpoint callback function to perform any application-specific event handling that is required.
Parent topic:Event Handling