tsZCL_AttributeReportingConfigurationResponse

This structure contains information from a ‘configure reporting’ response.

typedef struct
{
    teZCL_CommandStatus  eCommandStatus;
    tsZCL_AttributeReportingConfigurationRecord
                  sAttributeReportingConfigurationRecord;
}tsZCL_AttributeReportingConfigurationResponse;

Where:

  • eCommandStatus is an enumeration representing the status from the response (see Section 7.1.4).

  • sAttributeReportingConfigurationRecord is a configuration record structure (see Section 6.1.5), but only the fields u16AttributeEnum and u8DirectionIsReceived are used in the response.

Parent topic:General Structures