tsZCL_DefaultResponse

This structure is contained in a ZCL event of type E_ZCL_CBET_DEFAULT_RESPONSE (see Section):

 typedef struct PACK {
     uint8  u8CommandId; 
     uint8  u8StatusCode;
} tsZCL_DefaultResponse;

Where:

  • u8CommandId is the ZCL identifier of the command that triggered the default response message

  • u8StatusCode is the status code from the default response message (0x00 for OK or an error code defined in the ZCL Specification - see Section 4.2)

The above structure is contained in the tsZCL_CallBackEvent event structure, detailed in Section 6.2, when the field eEventType is set to E_ZCL_CBET_DEFAULT_RESPONSE.

Parent topic:General Structures