Compile-time options

This section describes the compile-time options that may be enabled in the zcl_options.h file of an application that uses the Touchlink Commissioning cluster.

The Touchlink Commissioning cluster is enabled as follows:

  • Touchlink - To enable the cluster, define CLD_ZLL_COMMISSION, then:

    • to enable the cluster as a server, define ZLL_COMMISSION_SERVER

    • to enable the cluster as a client, define ZLL_COMMISSION_CLIENT

  • Commissioning Utility - To enable the cluster, define CLD_ZLL_UTILITY, then:

    • to enable the cluster as a server, define ZLL_UTILITY_SERVER

    • to enable the cluster as a client, define ZLL_UTILITY_CLIENT

Parent topic:Touchlink Commissioning Cluster