eCLD_ZllCommissionCommandFactoryResetReqCommandSend

teZCL_Status eCLD_ZllCommissionCommandFactoryResetReqCommandSend(
    ZPS_tsInterPanAddress *psDestinationAddress,
    uint8 *pu8TransactionSequenceNumber,
    tsCLD_ZllCommission_FactoryResetReqCommandPayload
    *psPayload);

Description

This function is used to send a Reset to Factory New Request command to ask a remote node to return to its ‘factory new’ state. The command is sent as an inter-PAN message.

You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.

Parameters

  • psDestinationAddress                Pointer to stucture containing PAN ID and address information for target node

  • pu8TransactionSequenceNumber        Pointer to a location to store the Transaction Sequence Number (TSN) of the request

  • psPayload        Pointer to structure containing payload data for the Reset to Factory New Request command (see Section 44.8.10)

Returns

  • E_ZCL_SUCCESS

Parent topic:Touchlink functions