eCLD_ZllCommissionCommandScanReqCommandSend
eCLD_ZllCommissionCommandScanReqCommandSend(
ZPS_tsInterPanAddress *psDestinationAddress,
*pu8TransactionSequenceNumber,
tsCLD_ZllCommission_ScanReqCommandPayload
*psPayload);
Description
This function is used to send a Scan Request command to initiate a scan for other nodes in the local neighbourhood. The command is sent as an inter-PAN message.
You are required to provide a pointer to a location to receive a Transaction Sequence Number (TSN) for the request. The TSN in the response is set to match the TSN in the request, allowing an incoming response to be paired with a request. This is useful when sending more than one request to the same destination endpoint.
Parameters
psDestinationAddress Pointer to stucture containing PAN ID and address information for target node(s)
pu8TransactionSequenceNumber Pointer to a location to store the Transaction Sequence Number (TSN) of the request
psPayload Pointer to structure containing payload data for the Scan Request command (see Section44.8.5)
Returns
E_ZCL_SUCCESS
Parent topic:Touchlink functions