tsZLL_CommissionEndpointClusterInstances

This structure holds information about the Touchlink Commissioning cluster instance on an endpoint.

typedef struct PACK
{
#if (defined CLD_ZLL_COMMISSION) && (defined ZLL_COMMISSION_SERVER)
    tsZCL_ClusterInstance sZllCommissionServer;
#endif
#if (defined CLD_ZLL_COMMISSION) && (defined ZLL_COMMISSION_CLIENT)
    tsZCL_ClusterInstance sZllCommissionClient;
#endif
} tsZLL_CommissionEndpointClusterInstances;

where:

  • s``ZllCommissionServer is a ZCL structure containing information about the Touchlink Commissioning cluster server instance (refer to Section 6.1.16).

  • s``ZllCommissionClient is a ZCL structure containing information about the Touchlink Commissioning cluster client instance (refer to Section 6.1.16).

Parent topic:Structures