Logo
25.09.00-pvw1
MCUXpresso SDK Project v: latest
Document Release Versions
25.09.00-pvw1
25.06.00
25.06.00-pvw2
25.06.00-pvw1
25.03.00
latest

Introduction

  • MCUXPresso SDK

Getting Started

  • Github Repository
  • Zip Package

User Guide

  • Drivers
  • Examples
  • Middleware
  • RTOS
  • Boards

Development

  • Build And Configuration System
  • Developing with MCUXpresso SDK

Releases

  • Release Notes
mcuxsdk
  • Docs »
  • Run a non-XIP (plain load) example application using J-Link/J-Trace
  • Open on Repo Report an issue

Run a non-XIP (plain load) example application using J-Link/J-Trace

This section describes how to configure EWARM if using a J-link/J-Trace debug probe, or a probe which has been programmed with J-link firmware.

  1. Select “J-Link/J-Trace” and “Use macro file(s)”.

  2. Unselect “Use flash loader(s)” to use SEGGER J-Link flashloaders. Then, click the “OK” button.

  3. In IAR, click the “Download and Debug” button to download the application to the target.

  4. The application is then downloaded to the target and automatically runs to the main() function.

  5. Run the code by clicking the “Go” button to start the application.

  6. The hello_world application is now running and a banner is displayed on the terminal. If this is not true, check your terminal settings and connections.

Parent topic:Run a demo application using IAR


Copyright 2025, NXP. Last generated on Jul 17, 2025 16:25+0200; branch release/25.09.00-pvw1, revision b64f8fe5049b66fd3bf22464fb88e71ddf73d6ec.