Hardware requirements
Mini/micro USB cable
EVKB-MIMXRT1050 board
Personal Computer
Board settings
UART hardware flow control on one board. The UART will send data to itself(loopback), and hardware flow control function will be enabled on this example. So, please make sure the correct connection for example.
Pin Name Board Location connect to Pin Name Board Location
LPUART_TX J22 Pin 2 ---------- LPUART_RX J22 pin 1
LPUART_CTS J23 Pin 3 ---------- LPUART_RTS J23 Pin 4
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
This is LPUART hardware flow control example on one board.
This example will send data to itself and will use hardware flow control to avoid the overflow.
Please make sure you make the correct line connection. Basically, the connection is:
LPUART_TX -- LPUART_RX
LPUART_RTS -- LPUART_CTS
Data matched! Transfer successfully.