Hardware requirements

  • Mini/micro USB cable

  • EVKB-IMXRT1050 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of snvs example in the terminal window:

SNVS LP SRTC example:
RTC date and time has been synchronized with SRTC
Set up time to wake up an alarm.
Current datetime: 2014-12-25 19:00:00
Please input the number of second to wait for alarm and press enter
The second must be positive value
Alarm will occur at: 2014-12-25 19:00:16

 Alarm occurs !!!! Current datetime: 2014-12-25 19:00:16
Please input the number of second to wait for alarm and press enter
The second must be positive value