Hardware requirements
Mini/micro USB cable
Two MIMXRT1060-EVKB boards
Personal Computer
Board settings
To make the example work, connections needed to be as follows:
SLAVE connect to MASTER
Pin Name Board Location Pin Name Board Location
SOUT SW2-2 SIN SW2-3
SIN SW2-3 SOUT SW2-2
SCK SW2-1 SCK SW2-1
PCS0 SW2-4 PCS0 SW2-4
Note: Please start up slave example then connect PCS0(SW2-4) and start up master example, otherwise the high level signal from master board will affect the boot of slave board.
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
You can see the similar message shows following in the terminal if the example runs successfully.
FlexIO SPI interrupt example
Slave is working...
Slave runs successfully!