Hardware requirements
Mini/micro USB cable
MIMXRT1060-EVKB board
Headphone(OMTP standard)
Personal Computer
Board settings
J34, headphone connected
connect FLEXIO pins to the pad close to J23 as follows:
Pin Name Board Location Pin Name Board Location
RX_DATA J16-1 RX_DATA J23-11
TX_DATA J16-2 TX_DATA J23-17
SYNC J33-4 SYNC J23-16
BCLK J33-3 BCLK J23-23
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
Note: This demo uses both headphone mic and board main mic(P1) as input source. The headphone mic provides left channel data, and main mic (P1) provides right channel data. If users found there is noise while do record operation, most probably it is the headphone standard issue (OMTP and CTIA standard difference). You should use the OMTP standard headphone. You can disable the left channel by using an headphone without microphone feature.
When the demo runs successfully, the log would be seen on the OpenSDA terminal like as below.
~~~~~~~~~~~~~~~~~~~~~
FLEXIO_I2S interrupt example started!
FLEXIO_I2S interrupt example finished!
~~~~~~~~~~~~~~~~~~~~~
Note:
This example's right/left channel data is swapped due to the buffer maintain issue. This issue will be fixed in later release.