Hardware requirements
Mini/micro USB cable
MIMXRT1060-EVKB board
Personal Computer
Headphone(OMTP standard)
CS42448 Audio board(Not necessary if use on board codec)
Board settings
For Audio board: 1.Insert AUDIO board into J23 if on board codec is not used 2.Uninstall J41 For on board codec: 2.Make sure J41 is installed
Prepare the Demo
Note: As the EVKBMIMXRT1060 support two codecs, a default on board WM8960 codec and another codec CS42448 on audio board, so to support both of the codecs, the example provide options to switch between the two codecs,
DEMO_CODEC_WM8960, set to 1 if wm8960 used
DEMO_CODEC_CS42448, set to 1 if cs42448 used Please do not set above macros to 1 together, as the demo support one codec only.
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board. Steps for WM8960:
Insert the headphones into the headphone jack on MIMXRT1060-EVKB board (J34). Steps for CS42448:
Insert the headphones into the headphone jack J6 and line in line into J12 on the audio board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
Note: This demo uses both headphone mic and board main mic(P1) as input source of WM8960. The headphone mic provides left channel data, and main mic (P1) provides right channel data. If users found there is noise while do record operation, most probably it is the headphone standard issue (OMTP and CTIA standard difference). You should use the OMTP standard headphone. You can disable the left channel by using an headphone without microphone feature.
When the demo runs successfully, you can hear the tone and the log would be seen on the OpenSDA terminal like:
SAI example started!
SAI example finished!