Hardware requirements
Mini/micro USB cable
Loopback network cable RJ45 standard
MIMXRT1170-EVKB board
Personal Computer
Board settings
If Rx frame CRC error occurs, try to populate a suitable C66. The REV C/C1 boards populate 22pF which is high and may result in CRC errors on some of boards, if this is the case C66 may be removed or replaced by a smaller capacitor.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Insert loopback network cable to Ethernet RJ45 port(J4).
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Make loopback cable: 568B standard Unknowed standard J1 orange+white green+white J2 orange green J3 green+white orange+white J4 blue brown+white J5 blue+white brown J6 green orange J7 brown+white blue J8 brown blue+white
Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to 568B standard or the other standard. If your cable’s color order is not showed in the list, please connect J1~J8 based on your situation.
Running the demo
When the demo runs, the log would be seen on the terminal like:
ENET multi-ring txrx example start. The 0 frame transmitted from the ring 0 ! The frame received from the ring 0, 1, 2 is 1, 0, 0 now! The 1 frame transmitted from the ring 1 ! The frame received from the ring 0, 1, 2 is 1, 0, 1 now! The 1 frame transmitted from the ring 2 ! The frame received from the ring 0, 1, 2 is 1, 1, 1 now! …… The 9 frame transmitted from the ring 0 ! The frame received from the ring 0, 1, 2 is 0, 0, 0 now! The 10 frame transmitted from the ring 1 ! The frame received from the ring 0, 1, 2 is 0, 0, 0 now! The 10 frame transmitted from the ring 2 ! The frame received from the ring 0, 1, 2 is 0, 0, 0 now!
30 frames transmitted succeed! 10 frames successfully received from the ring 0! 10 frames successfully received from the ring 1! 10 frames successfully received from the ring 2!