Hardware requirements

  • Mini/micro USB cable

  • MIMXRT1170-EVKB board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

SSARC Software Trigger Example Start. Open the LED. Please press any key to trigger save operation. Saving. Please Wait. Closed the LED. Please press any key to trigger restore operation. After restoring, the LED will be re-opened. Restoring. Please Wait. SSARC Software Trigger Example Finish.